Motor_Stop_Trigger_Max_Position

Motor_Stop_Trigger_Max_Position

Address: 8788 (2254H)
Type: DWORD
Access: Read/Write
Unit: Motor steps
Range: -2147483648 to 2147483647
Default Value: 0
Store Supported: No
Description: It defines the max position used to filter the stop trigger signal. See Motor_Stop_Trigger_Options for more details.
Notes: --